PLUS+1 User Forum

PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: Marbek_Elektronik on December 21, 2023, 07:37:14 PM

Title: Curved Monitor usefull ?
Post by: Marbek_Elektronik on December 21, 2023, 07:37:14 PM
Hi,
I have a HP 30" Monitor.
I am thinking about curved monitor as computer players use.

Does anyone use such a monitor?

I think, the plane one is better than a curved one.
Title: Re: Curved Monitor usefull ?
Post by: Lukey on December 22, 2023, 03:23:40 AM
Cured monitors I think they are overrated/a gimmick, personally I use 3x 27".

Great for multi tasking, for example viewing, Guide, service tool and a data sheet
Title: Re: Curved Monitor usefull ?
Post by: Tor on December 22, 2023, 07:59:31 AM
Hello,

Can we keep this as a discussion if curved monitors are useful when developing in PLUS+1 GUIDE I will keep it here. In other cases I will move it to the "Off Topic" section.

For GUIDE developing I believe it can be a good thing. Large drawing on the screen, and everything at the same distance to your eyes. Your eyes don't have to re-focus as much when you are turning your head?  This is what I think, I don't have any facts to back me up.

The curved monitor has become a standard in our office, but myself are using two 27" flat monitors and a laptop screen. I thought it got a little crowded running both Service Tool and GUIDE on the same monitor. And if I wanted the same setup as I have now, I would have to get a 49" curved monitor (If I remember correct) and that was not an option.


Have a nice Holiday.