PLUS+1 User Forum

PLUS+ Tools => PLUS+1 GUIDE => Topic started by: acmall on July 30, 2020, 09:08:35 AM

Title: Guide 12.1 7 Complie Break Lockup
Post by: acmall on July 30, 2020, 09:08:35 AM
Has anyone experienced Guide 12.1.7 locking up if you click Break during a compile?

I have had this happen a few times on my desktop and laptop and had to kill the Guide process. Most concerning is that twice now this has resulted in the .scs file being deleted so the project was effectively lost. Fortunately I as able retrieve a recent copy so did not loose to much work?

Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: FStelzer on July 30, 2020, 11:47:43 AM
I've had the same issue today ..
Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: TheTurfDude on July 31, 2020, 04:24:54 PM
I have had this issue as well. I have found that if I click break while the compile progress message is "Refreshing Project" or anything before that message GUIDE will crash. If I wait until "Refreshing project" is done it seems to break the process ok.
Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: Fredrick on August 01, 2020, 04:37:11 PM
Yes, same issue here as well.
Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: deaks57 on August 02, 2020, 11:41:40 PM
Same...
Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: tjozmin on August 05, 2020, 10:20:47 PM
I have the same issue
Title: Re: Guide 12.1 7 Complie Break Lockup
Post by: Stefan on August 07, 2020, 11:50:42 AM
Hi,

This issue is reported and will be fixed as soon as possible.

Best regards
Stefan, PLUS+1 Helpdesk