Author Topic: SIM cards and configuration  (Read 12402 times)

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
SIM cards and configuration
« on: September 16, 2016, 01:51:04 AM »
What are you all doing in regards to SIM cards and configuration for the WS40x and WS50x units?  We're just getting past our first few, and so far the plan is to continue with the Proemion SIM cards since they happen to also have the servers.  Has anyone been using just run of the mill Tmobile or others such as from your cell phones?  If so, was doing the configuration a hassle at all?
Controls Engineer
Hydra-Power Systems

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: SIM cards and configuration
« Reply #1 on: September 16, 2016, 10:12:43 AM »
Hello FluidPowerTom,

we have already set up a telematics unit with a local SIM card provider.
The only thing you have to do is to change the APN setting which is done very fast.


Regards,
FStelzer

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Re: SIM cards and configuration
« Reply #2 on: September 16, 2016, 08:51:45 PM »
I was just thinking about this and wondering my self. I received our first WS403 yesterday. I forgot I needed to get a sim card. We were going to get a sim card from Verizon Wireless so we could add it to the company bill but Verizon Wireless is not listed in the configuration. Can you use ANY sim card from any company?

Thanks,
Mike

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: SIM cards and configuration
« Reply #3 on: September 16, 2016, 10:06:01 PM »
It's got to be a SIM card that uses GSM technology instead of CDMA.  Verizon and Sprint are two that use CDMA, so SIM cards for them won't work is my understanding.  AT&T and TMobile use GSM, so they're the main providers whose cards will work.
Controls Engineer
Hydra-Power Systems

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Re: SIM cards and configuration
« Reply #4 on: September 19, 2016, 02:30:45 PM »
Over the weekend I picked up a net10 sim card which contained sim cards for att and tmobile. I found the configuration page for net 10 for use with AT&T however the information listed doesn't match anything on the pre-filled APN network provider list. How do I go about getting these settings onto the WS403? Am I missing something that I need to get setup first with Proemion?

I am getting a double green flash then a single green flash then a solid red after a few minutes.

Thanks,
Mike Aalderink
« Last Edit: September 19, 2016, 02:32:31 PM by mikeaa12 »

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: SIM cards and configuration
« Reply #5 on: September 20, 2016, 08:44:26 AM »
Hi Mikeaa12!

I would be happy to help you out if you could send us more details to plus+1helpdesk@danfoss.com;

- I guess you are in the United States? Which one of the network providers did you choose in the list (see picture)? 
- Which LED on your WS403 is flashing?
- Are the sims using CDMA, GSM/GPRS/EDGE or UMTS/HSDPA?

Best regards
Nilla
PLUS+1 Helpdesk team

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: SIM cards and configuration
« Reply #6 on: September 23, 2016, 02:52:41 PM »
Hi all!

The configuration info below is what’s necessary, some or all of the fields may be left blank. In general, if you don’t know\have the value, leave the variable blank.  You should be able to get this info from the SIM card supplier.

  • SIM PIN
  • Network Code
  • ISP Username
  • ISP Password
  • Primary DNS
  • Secondary DNS
  • APN
  • SMS Service Center

There is a database of suppliers in the configuration tool, but it’s always good to ask when you buy the card. These settings can be configured individually when the automatically populated ones are not available, simply choose the variable, input the new value, and choose Download All Entries.

Best regards
Nilla
PLUS+1 Helpdesk team

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: SIM cards and configuration
« Reply #7 on: September 23, 2016, 05:42:39 PM »
Nilla, that's handy to have that list of required parameters.  Thanks
Controls Engineer
Hydra-Power Systems

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Re: SIM cards and configuration
« Reply #8 on: September 30, 2016, 02:24:48 PM »
FStelzer,

What SIM card have you been using? I grabbed and setup a NET10 GSM sim card labeled to work for AT&T and haven't been able to get any configurations to work.

Thanks,
Mike

//Edit I got the SIM card to configure to the point it is flashing single green then solid green. Seems to want to connect but not fully connecting to the server... Still working on this part.
« Last Edit: September 30, 2016, 05:47:19 PM by mikeaa12 »

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +2/-0
    • Trebro Turf Equipment
Re: SIM cards and configuration
« Reply #9 on: March 20, 2017, 05:36:03 PM »
Hello all,

Which SIM card/SIM carrier would be recommended for speed? I see and understand that GSM is the only option but does not that mean that 3G is the fastest network speed the Telematics device is capable of? We have been using the WS-503 unit and supplying them with the Proemion sold "M2M air" SIM card. Reading online that UMTS is supposed to be much faster download speeds than GSM

Thanks,

Jake
« Last Edit: March 20, 2017, 05:56:28 PM by Beezkneez »

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: SIM cards and configuration
« Reply #10 on: April 03, 2017, 01:19:01 PM »
Hi Jake!

I can't really recommend a specific SIM carrier but I can confirm that a WS503 does support GSM/GPRS/EDGE (class 10 [MHz] 850/900/1800/1900) and UMTS/HSPA (six band [MHz] 800/850/900/1700/1900/2100 [MHz]). Meaning 3G is the fastest available net speed today. More details on the hardware itself can be found here;

http://powersolutions.danfoss.com/solutions/telematics/ws503/#/

Best regards
Nilla
PLUS+1 Helpdesk

Offline turboshad

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +3/-0
Re: SIM cards and configuration
« Reply #11 on: July 19, 2017, 07:51:49 PM »
I've used the following on a WS403

Canada

Telus:
ISP Username - Leave blank
ISP Password - Leave blank
UMTS - sp.telus.com

Bell:
ISP Username - Leave blank
ISP Password - Leave blank
UMTS - pda.bell.ca

United States

AT&T Go Phone prepaid:
ISP Username - guest
ISP Password - guest
UMTS - phone

Cingular:
ISP Username - ISP@CINGULARGPRS.COM
ISP Password - CINGULAR1
UMTS - ISP.CINGULAR
« Last Edit: July 19, 2017, 07:53:42 PM by turboshad »