PLUS+1 Hardware > PLUS+1 Compliant Hardware
PVE-CC not responding to commands on CAN network.
ET:
OK, where should I start looking?
A number stamped somewhere on the valve or...?
Neil:
It's time to get oily Mr ET :o
The spools are stamped on the handle end.
Or as stated before there may be a valve id on the endplate, opposite end to the pressure and tank inlet.
You may be able to get the valve build in its entirety.
regards Neil
George:
--- Quote from: slewis on May 29, 2013, 06:44:03 PM ---Sauer-Danfoss has pre-made spool profiles that can be imported into the spool data page. If you can find out what spool is in that section I can send you the profile (I'll also need to know what node ID it is). If you can't find the spool part number, I may be able to track it down from the complete valve assembly number.
--- End quote ---
Is there a library of spool profiles or do we need to contact Danfoss every time we install / replace a PVED
The tools are OK, but documentation is a bit limited, IMHO :)
slewis:
George,
I haven't seen a library of spools profiles available for public download, which there should be IMHO. I've just asked my Danfoss rep. every time I run across a new spool, and built up my own library.
Navigation
[0] Message Index
[*] Previous page
Go to full version