Does anybody else have issues with the RTC adjusting itself on the dM1000?
In the HWD files there was new features to add timezone, and "Auto" adjust.
Even if the "Auto" is False, if i adjust the RTC it automatically change after an hour or so after i set new time...
i see in the latest HWD 321 template they have removed the option with timezone and "auto"