Recent Posts

Pages: 1 ... 4 5 [6] 7 8 ... 10
51
PLUS+1 Service Tool / Change params from a display instead of from Service Tool
« Last post by Hanshamsjel on April 25, 2023, 12:06:29 PM »
Hi,
often there is a p1d file to interact with a system component (pump/valve controller, etc)and that's where you set parameters, e.g. for tuning and limits. Is it possible to do this from a display instead ? What I mean is to send some sort of message in the same format as Service tool does. Or is it hard coded already, that a certain component controller will only communicate with Service Tool ?
Cheers
Hans
52
Code sharing / Re: String Concatenate C Code POU
« Last post by AlbertMilani on April 24, 2023, 03:46:30 PM »
Hi,

I can't seem to drive a bus with this output.  I can get it to work by first connecting a constant to the bus member and then connecting the StrConcat output to the same bus member but this is disturbing.  Am I doing something wrong?

Thanks in advance for any help,
Albert
53
License / Re: Renewal of license
« Last post by FluidPowerTom on April 21, 2023, 05:40:37 PM »
I have also had multiple customers have issues with express license renewal.  It is extremely vexing especially because most of them are only using it for the full version of the Service Tool which is included.
54
License / Renewal of license
« Last post by Jakob on April 21, 2023, 05:09:34 PM »
Hi helpdesk,
My license has gone and run out of maintenance periode, and now I would like to extend my license so I can keep doing things in guide.
So I clicked the link "Extend Maintenance", filled out the web form and confirmed the e-mail.
But that was a week ago, how long does it usually take to renew a license?

Hopefully I get it before my express license runs out.

BR. Jakob
55
Controllers / Re: SC024 Output problem
« Last post by G30RG3 on April 21, 2023, 02:15:37 PM »
Disconnecting just the ground wire will probably do just the same.
I would not be surprised if this is the case for all controllers, not just the SC024
56
Controllers / Re: SC024 Output problem
« Last post by Fredrick on April 20, 2023, 07:12:37 PM »
Yea, it sounds very dangerous.
But I think this is more related to your PLUS+1 code and not to the SC024, I have been using SC024, SC050, MC050-155 for years and never had this problem.
Interrupted CAN-bus does´t turn on the outputs if you not have programmed it to do that.

Could you show us your SCS file?

57
Controllers / Re: SC024 Output problem
« Last post by macbahi on April 18, 2023, 08:18:14 PM »
Hi!!

I did another test by disconnecting only the two CAN bus wires and the ground wire.
As a result all outputs turn ON.  In my opinion what is produced is very dangerous.

I wait with patience any feedback.

With best regards

58
Controllers / SC024 Output problem
« Last post by macbahi on April 18, 2023, 06:47:04 PM »
Hi!

I use SC024. It's work good.  But the big problem when I disconnect Connector 1 (gray) All output in Connector 2 (Black) turn ON.

Please have you idea about this problem.

Thanks in advance for your help
With bests regards
59
Controllers / Re: SC050 CAN1 problem
« Last post by macbahi on April 18, 2023, 06:38:19 PM »
Thanks sir
60
Displays / Re: DM430 new hardware file
« Last post by jlindholm on April 18, 2023, 11:04:30 AM »
Hello.
The legacy HWD files for migration of DP2x0 to DM430 are available in the release candidate style (there are minor errors in some of the templates).
However if you are in big need and wants to use the HWDs please contact PLUS+1 Helpdesk by creating a case at http://plus1helpdesk.danfoss.com and ask for the legacy Dm430 HWDs.
The HWDs will not be added to PLUS+1 Update Center to avoid mismatch with the DM430 HWDs used for new program development.

Jonas Lindholm
PAE Manager
Pages: 1 ... 4 5 [6] 7 8 ... 10