Recent Posts

Pages: 1 [2] 3 4 ... 10
11
PLUS+1 Service Tool / Looking for connecting to PVED-CC Serie 4
« Last post by Stephane on January 19, 2023, 04:53:42 PM »
Hello,

I want to connect to a valve PVED-SS Serie 4
Accordinf to the pdf, i must download the PLUS+1 PVE Service tool S4 DJ ref 11103046.
But i can't find it on danfoss.com

I download the PLUS+1 Service Tool 2022.4.
But i was only able to download the p1d file for the PVED-CC serie 5.

Is there any solution?

Best regards.
12
Off topic / Con Expo 2023
« Last post by FluidPowerTom on January 18, 2023, 06:20:56 PM »
Will a goodly chunk of Danfoss PLUS+1 / Electronics people be at Con Expo this year?  I know we've got some pretty big (for us) PLUS1 customers with booths there that I'll be connecting with, but I wouldn't mind connecting with some Danfoss folks as well.  Feel free to send me a PM if you want to get together.  Personally, I'll just be there 3/16 and leaving 3/18.
13
General controls / Re: Set Pulse by Service tool
« Last post by Camox on January 17, 2023, 09:28:48 AM »
Hello,
Thanks for your response.
I make test. The SetPulse component is only available in advanced page.

Good day
14
PLUS+1 Compliant Hardware / Re: Using Sensor_3Pt with Joystick JS6000
« Last post by macbahi on January 17, 2023, 05:04:46 AM »
Hello

Here is calculation detail see picture.

From those calculates I think the range and unit of sensor_3Pt are 10000 and 0.01.

Both real and calculate result are the same.

With bests regards 
15
PLUS+1 Compliant Hardware / Re: Using Sensor_3Pt with Joystick JS6000
« Last post by macbahi on January 16, 2023, 09:00:26 PM »
Hello

It's me again.

Sorry in picture was mistake  1000 is 20% 0.2   and 2000 is 40% 0.4 and  3000 is 60% 0.6

Tank you

Best regards
16
PLUS+1 Compliant Hardware / Re: Using Sensor_3Pt with Joystick JS6000
« Last post by macbahi on January 16, 2023, 08:40:58 PM »
Hello sir

Thank you very much for your answer but I am not satisfied with your calculations because first your formulas is different than in Sensor_3Pt remark.
This is Danfoss problem. 

First the formulas are different in manual and in plus+1 guide. 
The second Mid Dbnd% and Hi/Lo Dbnd% their range is 5000 but their unit is 0.01%.   I think it must be 0.02%.
It not possible to be same as LoCal% or MidCal% or HiCall and Fault because their range is 10000  and their unit is 0.01%

In my case if I use Plus+1 guide sensor_3Pt with the yellow remark formula with unit=0.02 as shown in my last picture I found good result as my joystick real measure.  You can see the picture below.

As conclusion
There are some mistake in manual and in plus +1 guide formula.
The plus+1 guide sensor_3Pt remark formula is correct but the unit is not correct.  It's most be 0.02.
Or keep the unit 0.01% but change range from 5000 to 10000.  Depending how it's programmed inside.

I hope Danfoss corrects its mistakes in the future

I also hope that this exercise is beneficial for other users.

With best regards



17
General controls / Re: Set Pulse by Service tool
« Last post by FluidPowerTom on January 16, 2023, 05:33:06 PM »
Whenever I've used the Set Pulse component I trigger it using a button in an Advanced Service Tool page.  I don't recall if you can do it in a Basic page or not.
18
PLUS+1 GUIDE / Re: Certificate IEC 61508 PLUS+1 Dev Tools
« Last post by Nickyk on January 16, 2023, 04:06:21 PM »
Hello Tor,

Thanks, very happy with the update. I have switch to 2021.2 in the mean time  :D
19
Controllers / Re: SC050-020 Digital Out Errors
« Last post by Nickyk on January 16, 2023, 03:51:48 PM »
Hi Scott,

Good idea to start a new thread, I have the same issue but with different hardware SC050-122. For me the fix from Tor is also not working only reducing. I also noticed that some pins are more sensitive to produce a status bit 8 error than others.
I will try your solution as well, but this isn't a fix which is going to work for me in order to be compliant with the requirements from the functional safety standard. I'm also in contact with Danfoss to solve this issue. I will post my findings as well.
20
PLUS+1 Compliant Hardware / Re: Joystick JS6000 address problem
« Last post by macbahi on January 16, 2023, 02:44:29 PM »
Hello Sir Acmall,

It's done. I was very easy.  Thank you very much.

Now I know my error.  I opened your file with Plus+1 guide viewer to have idea about your program.  I was see the program and it was not easy to understand.

But after your last message I opened it with service tools.  I found it easy and It's done.  Sorry for confuse.

Thank you very much for all help

With best regards
Pages: 1 [2] 3 4 ... 10