Recent Posts

Pages: [1] 2 3 ... 10
1
PLUS+1™ Service Tool / Monitoring inputs
« Last post by matttargett4 on Today at 08:28:36 PM »
Hi,

I’m building a basic application and to verify it’s working correctly I would like to be able monitor how inputs and outputs vary as I adjust connected hardware, in my experience with other plc stuff there is usually a monitoring mode where you can simply see your program and how it behaves in real time.

Is there something like this I can do? Or some other way of achieving what I’m after?

Thanks

Matt
2
Controllers / Re: Hydrostatic pump controller
« Last post by tronelec on Today at 06:06:53 PM »
in my experience the problem will be the other way around if the actuator is 24 volt and your source is 12 volt, but the actuators for pumps consume very little current, if you don't over do the current there would be no problem, what if the curve changed relationship between current versus flow
3
Controllers / Re: Hydrostatic pump controller
« Last post by matttargett4 on Today at 12:27:05 AM »
Thanks,

That’s kind of what I was wondering, yes I’m using a 90l130 with edc control set up as 14-85mA and kind of wondered if the Pwm would take care of it, so in your opinion 24vdc supply voltage is fine? I guess I should connect both coils for as much impedance as possible?

Thanks

Matt
4
Controllers / Re: Hydrostatic pump controller
« Last post by deaks57 on January 20, 2022, 12:54:48 AM »
If you are driving a 90S EDC (KA) then never put 12V directly to it. You don't need more than 2.5V to get to max flow. Anything >6-7V increases service business ($$$).
If you are using a 90S EDC compliance block with the currents set correctly (14-85mA) then you don't need to worry about supply volts. The PWM duty shifts accordingly to control the current.
5
Controllers / Re: Hydrostatic pump controller
« Last post by G30RG3 on January 19, 2022, 10:59:55 AM »
The resistance of a 12V coil is typically below 4 Ohm, for a 24V coil we're talking about 15 to 20 Ohm.
This means that were you planning to use a 12V coil on a 24V  system, you would have a peak current of 6+ A.
This gets worse if your voltage rises to 27-28V (on mobile machines).

Depending on the type of pump, you might be able to change the coils to the rated voltage. To me, that's the preferred option.
Second option is to bring the controller to 12 Volt supply.
If that also is not an option, one could opt to install shunt resistors to limit the current peaks but that might might cause other issues as you probably need a +1.5 A max current to get the pump on max displacement. With a shunt in the region of 12 Ohm, that would mean a resistor that takes 20-25 Watt .
6
Controllers / Re: Hydrostatic pump controller
« Last post by matttargett4 on January 18, 2022, 11:10:00 PM »
Another question about software settings and hardware

My vehicle is 24v, so the controller supply voltage will be 24v, the edc control is 12v, how would I take care of that? Can it be done or do I need a 12v supply voltage?

Thanks

Matt
7
Controllers / Re: Hydrostatic pump controller
« Last post by matttargett4 on January 18, 2022, 04:48:18 PM »
That's worked,

Thanks for your help!
8
Controllers / Re: Hydrostatic pump controller
« Last post by TheTurfDude on January 18, 2022, 04:08:06 PM »
Hello,

When using a function block that connects to an output pin you need to delete the config settings for that pin in the outputs page (see screenshot). CurrentOut and OutputMode are both being set with the values from the function block, so the constant values that are connected in the output pages must be deleted or they will interfere. Delete the constant values (as shown in the screenshot) for both C2p03 and C2p04.

Hope that helps.
9
Controllers / Hydrostatic pump controller
« Last post by matttargett4 on January 18, 2022, 03:47:16 PM »
Hi,

I'm looking to make a control module which will take a joystick input and transfer that to a hydrostatic pump output.

I'm using the MC024-120 controller and a S90 EDC pump.

I've connected up the modules as best as I know how in the Plus1 Guide software , but when I try to compile the project, a number of errors come up, shown below. Also attached the project file if that's any use.



Any help would be greatly appreciated

Thanks
10
PLUS+1™ Service Tool / E322 access denied to parameter
« Last post by dudleyr on January 17, 2022, 09:14:23 PM »
Hello,

I am getting error "E322: Access denied to parameter" when trying to update a parameter while logged in remotely to a machine via RP1210. This is something we do regularly with our machines, but it is not working on this machine.

I am also getting a "Read-Only Access" message for the Safety Status in the PLUS+1 Remote Connection Status dialog (see attachment), even though I have switched the telematics device to be in Realtime mode.

Any idea what could be causing this? Or how to determine whether it is a Service Tool or a telematics device issue?
Pages: [1] 2 3 ... 10