PLUS+1 User Forum

PLUS+1™ Software => Telematics => Topic started by: Loader on September 10, 2015, 02:12:28 PM

Title: CAN informations view
Post by: Loader on September 10, 2015, 02:12:28 PM
Hi, is there a method to view the messages on CAN bus? For example like CanKing?
Thanks!
Title: Re: CAN informations view
Post by: spittet on September 10, 2015, 06:24:17 PM
Why not use CANKing? It's designed exactly for this.

Sam
Title: Re: CAN informations view
Post by: Loader on September 11, 2015, 09:28:44 AM
Hi Spittet, when I use Telematic hardware I don't see anything on CAN bus with CANKing!!
I something wrong?
Thanks
Title: Re: CAN informations view
Post by: spittet on September 11, 2015, 06:34:36 PM
Ok, I didn't see that this post was related to Telematic. I have no clue on this one. Sorry.

Sam
Title: Re: CAN informations view
Post by: jashom1 on September 16, 2015, 08:30:32 AM
I have viewed Telematics data and Service tool data with CanKing and the CG150.

All you have to do is in the CAN Controller window under the Bus Parameters tab, un-tick "Exclusive" and tick "No init access" This then does not configure the CG150 to communicate but relies on the main program wether it's the Service Tool, or the Telematics configurator.  The catch here is you won't see anything until the service tool or Telematics configurator configures the CG150 for communication.

With this method you still can send messages too

I use it all the time.
Title: Re: CAN informations view
Post by: Loader on September 16, 2015, 02:12:04 PM
Thank you Jashom
I'll try with your tips!
Bye
Title: Re: CAN informations view
Post by: FluidPowerTom on November 06, 2015, 11:38:27 PM
If the other suggestion doesn't work then you might try CANMoon or, if you can find it, the old CANMoon Lite.  I seem to recall CANMoonlite working in situations like what you've described.