PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: Sergio-DEK on November 24, 2015, 12:03:18 PM
-
Hi!
I'm trying to connect with a MC024-024 controller using the service tool and suitable P1D file.
When I go online and scan the system it responds with status
(https://dl.dropboxusercontent.com/u/4978895/connection_warning.png)
Does anybody know what it means, or what should I do to connect normally?
Thnx
-
maybe you use a HW file "Beta"!
-
I agree with Loader.
This error Pops up, if there is a HW file on the Controller or better said a "Firmware" which is not released from Danfoss.
KR,
FStelzer
-
Thank you guys for the help. You are right.
I also contacted Danfoss support. They said that the program in the controller is a redesigned "Automotive on PLUS + 1" program made by Gehl/Manitou/Mustang and I'm trying to connect with a standard Danfoss diagnostic file (P1D). Finally I managed to connect and change the necessary parameters.
Regards,