PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: F.M.Elettromeccanica on October 10, 2020, 04:13:57 PM
-
Hallo gurus,
Is there a way to have a 5v DOUT DC on a MC050-110? I wish to avoid to install a DC/DC Converter...
Thanks in advance
-
Hi,
there is sensor power pin on c1p8 and sensor power ground on c1p9.
You can't switch it.
I believe, max current is 360mA.
-
If you did need a switchable 5 VDC out you'd have to use an output set to Duty Cycle control and reference the supply power along with a little math to make the duty cycle create a 5V output. In my experience you can keep it within 0.05 volts or even better accuracy. That said it's certainly not going to be a true regulated 5 V out like on pin 8.
-
Thanks everyone for the answers. In fact it is exactly what I did, only it seems that the problem is the frequency (max 4khz). I believe I will take a PWM / DAC converter to have an effective DC current
-
And please think about, that hardware couldn't output more than 5V, if there would be an software error!
Do you need a switchable 5V supply or do you need a voltage output between 0 and 5 V regulated? And what current?
-
Hi Marbek, I need a voltage regulation between 0 and 5V
500mA max
-
How many pieces every year?