Author Topic: DM1200T bluetooth  (Read 2594 times)

Offline jwestcott23

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
DM1200T bluetooth
« on: April 28, 2021, 08:44:22 PM »
Has anybody tried to use or connect to the bluetooth available on the DM1200T? I have the interface enabled, have it set to discoverable, and set autopairing to true just so that i could try to get connected to it. I had it show up on my phone as available only one time and when i tried to pair with it, i got a message on my phone that there is an app needed for pairing  ??? ? I was just wondering if anybody had some advice or maybe a sample that would help me.

Thank you!

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: DM1200T bluetooth
« Reply #1 on: April 29, 2021, 09:29:50 AM »
Hi,

I have not played around with the DM1200 and mobilephones enough to help you with this setting. Maybe someone else has a good answer.

Please contact the PLUS+1 Helpdesk and create a case if you still have problem:  https://danfoss.secure.force.com/dpscustomersupport
Add to the case what HWD file and what type of phone you are using, as much details you can.
Best regards,
Tor
PLUS+1® SW PAE Team