Recent Posts

Pages: 1 ... 8 9 [10]
91
PLUS+1 GUIDE / Re: Problem by installing 2024.1.3 with update center
« Last post by Marbek_Elektronik on February 12, 2024, 01:36:32 PM »
Has anyone installed it succesfull?
92
PLUS+1 GUIDE / Problem by installing 2024.1.3 with update center
« Last post by Marbek_Elektronik on February 10, 2024, 09:17:00 PM »
Hi,
I start update from update center and there comes the message "update center is running, please close it"
I close it in system tray and then comes: "Download on installation in process"

I can't solve this problem and Guide 2024.1 will not start.

What can I do?
Installation of service tool, same problem.
93
PLUS+1 Compliant Hardware / Re: Re: CG150-2 Connectivity Problems
« Last post by G30RG3 on February 10, 2024, 12:01:06 PM »
@tannnnn

Your question is in the wrong place, here, but to respond quickly:

You can use 2 of the 4 Prop/MF-outs to control the two coils, for instance by using the compliance block for a H1P pump, or using your own logic to directly feed the outputs, and use one of the 2 digital outputs to release the brake whenever the PWM-output is not equal to 0.
One issue you'll see is that the output pin names are not the physical pin numbers, depending on the cable / connector option chosen.

If you have a joystick with two 12-pin connectors:
X100p15, X100p16, X100p17 and X100p18 are connected to Pin 1 to 4 on the black connector.
X100p10 is Connected to pin 8 on the black connector, X100p20 is connected to Pin 7 on the Black connector.
Don't forget to connect both Pin 1 and Pin 6 on the grey connector to ground, and get the supply on pin 2, 7, 8 and 9 on the grey connector!
94
PLUS+1 Compliant Hardware / Re: JS1H - p1d file PWH js
« Last post by G30RG3 on February 10, 2024, 11:43:32 AM »
Sure tannnnn,

You can use 2 of the 4 Prop/MF-outs to control the two coils, for instance by using the compliance block for a H1P pump, or using your own logic to directly feed the outputs, and use one of the 2 digital outputs to release the brake whenever the PWM-output is not equal to 0.
One issue you'll see is that the output pin names are not the physical pin numbers, depending on the cable / connector option chosen.

If you have a joystick with two 12-pin connectors:
X100p15, X100p16, X100p17 and X100p18 are connected to Pin 1 to 4 on the black connector.
X100p10 is Connected to pin 8 on the black connector, X100p20 is connected to Pin 7 on the Black connector.
Don't forget to connect both Pin 1 and Pin 6 on the grey connector to ground, and get the supply on pin 2, 7, 8 and 9 on the grey connector!
95
General controls / Guide Ver 2024.1.3.5743
« Last post by dlewis on February 09, 2024, 06:57:16 PM »
I get the following message when trying to compile a display program that compiles fine using the previous version of Guide.

***ERROR 597 *** [PLUS1_IDE] Screen Editor Error: {Error Code201; Missing fonts: OCR A Extended [Bold]} >:(
96
Displays / Re: Rotate Text
« Last post by BRIan on February 09, 2024, 01:40:58 AM »
HaHa found it. See attached screen shot and other thread. (https://www.plus1forum.danfoss.com/index.php?topic=871.msg3570#msg3570)
97
Displays / Re: Rotate Text
« Last post by BRIan on February 09, 2024, 01:33:20 AM »
I've been searching for an answer to this too. Importing as a graphic only works if the text is static. If it varies, as in supply volts, that won't work.
98
Displays / Rotate Text
« Last post by dlewis on February 08, 2024, 05:27:51 PM »
I would like to use a DP720 in a portrait orientation rather than Lanscape.   Rotating any graphics is not an issue, but how do I rotate text?  There are even times when I'm using the display in the normal orientation in which it would be nice to rotate the text.

Any ideas, besides importing the text as a graphic?
99
General controls / Re: Application ID
« Last post by Lukey on February 08, 2024, 01:09:43 AM »
@FluidPowerTom
Bottom right of GUIDE, re select DEFAULT, this will reset the layout to standard.
100
General controls / Re: Application ID
« Last post by FluidPowerTom on February 07, 2024, 05:05:26 PM »
How do I bring that Inspector window back after it has somehow disappeared?  I can't see it to change my Application ID
Pages: 1 ... 8 9 [10]