Author Topic: Over voltage protection on the IO modules  (Read 7166 times)

Offline Rafal_Typiak

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +1/-0
Over voltage protection on the IO modules
« on: May 27, 2015, 03:31:59 PM »
Hello,
I've read somewhere (don't know where) that the MCs have overvoltage protection on their inputs. Am I correct?
If so than I was wondering if the same realtes to the IO modules? I'm probably going to have to put 24V sensor signal on the DIN pins which are 0-5V. Was wondering if their simply 5V tolerant or can they handle the Vcc?
My experience so far sais that the MCs can handle overcharging but what about the IO modules?

Best regards,
Rafa? Typiak

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Over voltage protection on the IO modules
« Reply #1 on: May 27, 2015, 04:07:43 PM »
Hi,
Can-shield input: normally max. 25V (OX024-110: 36V?)
All other inputs: normally max. 36V
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Rafal_Typiak

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +1/-0
Re: Over voltage protection on the IO modules
« Reply #2 on: May 29, 2015, 09:40:36 AM »
So they all have 36V over charge protection (apart from Can Shld)? Sweet. Thanks  :D

Rafa? Typiak