Author Topic: DST X800 - resolution  (Read 878 times)

Offline sverreo

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +1/-0
DST X800 - resolution
« on: March 14, 2023, 03:14:11 PM »
Hi,

I have a DST X800 (CANopen) i am currently testing. In the manual it states that the resolution can be changed using object 0x6005, and the default value should be 0x3E8 (1000dec).

The resolution is default 1mm/bit when i test it, and i'm trying to change it to 0,1mm/bit.

If i upload object 0x6005 i get value "1", and not 0x3E8:
 0    0000067F         8  40  05  60  00  00  00  00  00    2314.571350 T
 0    000005FF         8  42  05  60  00  01  00  00  00    2314.571940 R

Whatever i try and change the value to i get download error:
 0    0000067F         8  22  05  60  00  0A  00  00  00    2329.671760 T
 0    000005FF         8  80  05  60  00  02  00  01  06    2329.672440 R
 0    0000067F         8  22  05  60  00  E8  03  00  00    2336.407460 T
 0    000005FF         8  80  05  60  00  02  00  01  06    2336.408150 R
 0    0000067F         8  22  05  60  00  02  00  00  00    2352.923390 T
 0    000005FF         8  80  05  60  00  02  00  01  06    2352.924070 R

Have anybody here changed the resolutin on these CANopen sensors?

 


Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: DST X800 - resolution
« Reply #1 on: March 19, 2023, 08:31:03 PM »
Hi,

Try using a 2B or 2F in the write command.

67F 8 2B 05 60 00 E8 03 00 00