Author Topic: DP700 NUMERICAL TEXT  (Read 5569 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
DP700 NUMERICAL TEXT
« on: January 15, 2020, 01:44:15 AM »
hey Guys,

so for the DP700 displays, how do you create a numerical text?   before it was quite simple, I guess with this it is the same however I just cannot figure out how to do that. when I bring a text on the screen and check the properties I can adjust all that, properties of the text however I do not see a way to tell it will be showing a numeric value.

my thought is that I could use the text definition however the system tells me that my number is not a text and then I am stuck on that.

I apreciate any advise on this matter

Thanks

Offline SJ Industries

  • PLUS+1 Expert
  • ****
  • Posts: 60
  • Karma: +2/-0
Re: DP700 NUMERICAL TEXT
« Reply #1 on: January 15, 2020, 04:55:06 AM »
Page 442 of the manual explains how to add a numerical value to a text def. "%1$" and Add format.

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: DP700 NUMERICAL TEXT
« Reply #2 on: January 15, 2020, 07:05:44 PM »
my bad,

I was selecting the text from the selector section not from the project library...

nevermind

thanks SJ for the advise