Author Topic: MC018 C1p11 error 23 and 665  (Read 955 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +1/-0
MC018 C1p11 error 23 and 665
« on: May 01, 2024, 11:57:59 PM »
Hi Guys,

It's my first time I use MC018. I will use all output. Every think it's OK.
All setting output are the same way.
But when I compile the program, I get error only for C1P11.
You find enclosed the pictures of errors

I had update my plus+1 to 2024.1.5.

Thanks in advance

With best regards
Mac bahi

Offline A.Fitz

  • PLUS+1 User
  • **
  • Posts: 6
  • Karma: +0/-0
Re: MC018 C1p11 error 23 and 665
« Reply #1 on: May 02, 2024, 04:50:17 PM »
It looks like nothing is connected to the DigOut component based on the error.
I would use command "V" to view the connection and verify you have something driving it.

I would bet this is a copy paste error where you forgot to change the name somewhere to correlate to this pin.

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +1/-0
Re: MC018 C1p11 error 23 and 665
« Reply #2 on: May 08, 2024, 02:31:45 PM »
Hello Fitz

Thank you very much to answer me.
The error it's was feedback but plus+1 compiler show other thinks.
Since I installed the last version the compilation it's not as before.

Any way thanks sir.

With best regards
mac bahi