PLUS+1 Software > Communication
Transmit a J1939 data : PGN65128 SPN1638 (HydTemp)
(1/1)
spittet:
Hi,
I want to broadcast an information using J1939 protocol. I have an hydraulic temp sensor connected to one of the inputs of a MC050. I want to transmit this info in J1939. The device that want this info is waiting for data of PGN65128 and SPN1638.
I saw that there is a block in the J1939 Function Block named VF_Rx that is used to receive the same data. But I didn't found the one to transmit this data. Is there a generic J1939 transmitter block that I can simply input the data, the PGN, the SPN, the CAN port and the source address.
Let me know!
Sam
spittet:
After some search, I was able to do it. For future reference, here is how I did it :
-Use a "Transmit CAN" block.
-Set the "EXT" at true.
-Set the "RTR" at false.
-Set the length at 8.
-Create an array of 8 U8 bytes.
-Fill the byte0 with the hydraulic temp (from 0-250, 1°C = 1 step, -40°C offset)
-Fill all the other bytes with 255.
-use the following ID : 0x0CFE6803 (FE68 is the PGN 65128, 03 is the address of my MC050 ECU, 0C is the priority)
Voila!
Done!
I hope this will help people in the future!
Sam
Neil:
Great work Sam.
thank you for the info.
regards Neil.
Navigation
[0] Message Index
Go to full version