PLUS+1 Software > Displays

Download time in DM1000

(1/2) > >>

Camox:
Hello,
I work actually on software for DM1000 dysplay.
The download time for add a software in the dysplay in long. During the download the load speed on the dyspaly is 10kb/s.

We can change the load speed ?

Thank in in advance.

Good day

Tor:
Hello Camox,

Yes the download time for the DM1x00 displays are a bit longer than the rest of units. Especially when you are replacing the HWD file and OS.
I recommend to use USB when working with the DM1x00 displays. You will save a lot of time. When it take almost an hour downloading a new OS with CG150, it will only take a minute with the USB.

If you want to order you can find the part number in the image below (11231512). You can also find it in the Data Sheet.


Have a nice day.

Camox:
Hello Thor,
Thank a lot four your response.

I’ll get that cable fast.

Have a nice day

Camox:
Hello Thor,
Is it necessary to have a driver that the cable connection works?
Thanks

Tor:
Hello,

No, the drivers are included in the PLUS+1 Service Tool.
You need to use the Interlink Gateway.  See Image.

Have a nice day

Navigation

[0] Message Index

[#] Next page

Go to full version