Author Topic: Checkpoints not showing, only Servicetool.MasterPassword.Write  (Read 5071 times)

Offline swordfeather

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +1/-0
Hi,

In the servicetool only this one parameter is showing up for my MC050. "Servicetool.MasterPassword.Write"
I didn't use the piece of code to protect downloading parameters.

Anyone had this before who can help me?

Thx,

Regards

Swordfeather

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: Checkpoints not showing, only Servicetool.MasterPassword.Write
« Reply #1 on: June 10, 2022, 10:37:45 PM »
It sounds like you're editing and Parameter page instead of a Log Page.  There should be in the same list as the checkpoints all of the pin information such as C1p2.voltage...etc.
Controls Engineer
Hydra-Power Systems

Offline swordfeather

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +1/-0
Re: Checkpoints not showing, only Servicetool.MasterPassword.Write
« Reply #2 on: June 16, 2022, 10:14:00 PM »
True. :-X

-------------------Earth surface-----------------------------------------
                                .
                                .
                                .
                               \/
                      Me in shame


Thank you for the response.