PLUS+1 User Forum

PLUS+1 Hardware => I/O Modules => Topic started by: macbahi on October 25, 2023, 09:50:57 PM

Title: OX024-110 CAN1 problem
Post by: macbahi on October 25, 2023, 09:50:57 PM
Hello,
I usually use SC050 ou SC024 CAN0 with module OX024-110 Can0.  It's work very well.
But now I am changing my communication with CAN1.  So I can not see my module OX024 -110.
Please the CAN+ CAN-  of module OX024-110 can be CAN0 and CAN1.  Or only CAN0.

Thany your for your help
With best regards
Title: Re: OX024-110 CAN1 problem
Post by: Lukey on October 26, 2023, 02:39:54 AM
I can't comment from personally experience but the first thing that comes to mind;
In your SC GUIDE program have you changed the CAN address for the Expansion Module to CAN 1 ? as default is CAN 0 I believe.
Title: Re: OX024-110 CAN1 problem
Post by: macbahi on October 26, 2023, 02:38:58 PM
Thank you for your reply.
Finally it's correct but I don't know why In service tools the module OX024 is connect to CAN0 despite being connected to CAN1 in guide.
Please see image.  And also I can not see the SC050 secondary.
But it's working.
Thank you for your help

With best regards

Title: Re: OX024-110 CAN1 problem
Post by: FluidPowerTom on October 26, 2023, 04:16:20 PM
It's possibly because your CG150 is physically connected to CAN0?
Title: Re: OX024-110 CAN1 problem
Post by: acmall on October 31, 2023, 08:53:28 AM
The ECU list shows the port that you have connected to on each device. As the OX024-110 only has one CAN port this is showing as CAN 0.