14
« Last post by sverreo on March 14, 2023, 03:14:11 PM »
Hi,
I have a DST X800 (CANopen) i am currently testing. In the manual it states that the resolution can be changed using object 0x6005, and the default value should be 0x3E8 (1000dec).
The resolution is default 1mm/bit when i test it, and i'm trying to change it to 0,1mm/bit.
If i upload object 0x6005 i get value "1", and not 0x3E8:
0 0000067F 8 40 05 60 00 00 00 00 00 2314.571350 T
0 000005FF 8 42 05 60 00 01 00 00 00 2314.571940 R
Whatever i try and change the value to i get download error:
0 0000067F 8 22 05 60 00 0A 00 00 00 2329.671760 T
0 000005FF 8 80 05 60 00 02 00 01 06 2329.672440 R
0 0000067F 8 22 05 60 00 E8 03 00 00 2336.407460 T
0 000005FF 8 80 05 60 00 02 00 01 06 2336.408150 R
0 0000067F 8 22 05 60 00 02 00 00 00 2352.923390 T
0 000005FF 8 80 05 60 00 02 00 01 06 2352.924070 R
Have anybody here changed the resolutin on these CANopen sensors?