PLUS+1 User Forum
PLUS+1 Hardware => Displays => Topic started by: Loky1983 on December 05, 2013, 10:02:23 PM
-
Hi,
I am just wandering what does the visible option when you check the settings of
either texts or images
Thanks
-
According to the User Manual, Visible is an OUTPUT from the display screen. Here's the text from the user manual :
Outputs a True Boolean signal when a library item becomes visible.
To be visible, a library item must have a True Screen Area, a True Enable property, and a Priority that is higher than or equal
to the Priority of any other library item in the same Screen Area.
(You must connect a wire to the Data bus to be able to output this signal.)
I'm not sure if this is useful. I've never used it and I'm not sure I can see a utility to this feature. To me, it is visible when I see it on the real screen when I'm testing my display program. If I do not see it, either it's not enabled or either there is another thing that is enabled and higher priority that is in front of it.
Sam
-
That also what i thought that it wasn't that useful
cause as you said you enable it or not...
But anyway Thanks
-
I use the "Visible" attribute quite a bit in my terminal programming.
It works for a broad range of things depending on if you wish to display an object on a screen.
An example. When a button is pressed to do a function, a variable is set which will display a graphic with a warning. Sort of an "Are you sure?' thing.
We also have various options on different machines. If that option is turned on, some graphics and/or texts will be displayed, others not.
Another thing is a text list driven by a fault process, when a fault appears I have a pink graphic as well as a text list appear with the fault or faults displayed, otherwise it is a time display.
Everything has a purpose if you choose to use it or not is up to you.
Regards,
Brian Bandura
-
is the attribute "visible" and "enable" compiled like the following logic:
You see the text if "visible" AND "enable" is set ?
I think, you could use maximum two variables to activate the text.
This is wrong, what I have wrote 2014.
Enable is the only input to see the text.