PLUS+1 User Forum
PLUS+1 Hardware => Displays => Topic started by: Federico on August 16, 2013, 04:39:13 PM
-
Estimados, alguno podría indicarme cuales son las diferencias entre CAN R y CAN L?
Necesito comandar 2 motores Diesel y pienso utilizar un CAN0 para cada uno, el tráfico es independiente? La carga del Bus es la suma de cada carga?
Saludos
**************************************
Dear, someone could tell me what are the differences between "CAN0 R" and "CAN0 L"?
I need to commandeer two diesel engines and I use a CAN0 for each. Traffic is independent? The bus load is the sum of both load?
regards
-
Hello Federico,
The CAN0 R and CAN0 L are related to the REDCAN feature.
The software provides an interface to be able to use either pin set or both pin sets depending on the mode/configuration.
Both sets of pins can get connected to the same CAN0 Transciever, again depending on the mode/configuration.
If it is configured to use both sets of pins, they are effectively on the same bus and traffic is not independent.
I hope this helps.
Randy