Recent Posts

Pages: [1] 2 3 ... 10
1
General controls / Software System Simulation – Testing-as-a-Service
« Last post by Tor on May 19, 2022, 10:54:43 AM »
Hello,

If you are developing your own PLUS+1 Code? Please read the information below:

"For the last years Danfoss has been strongly developing its system simulation and testing capabilities, to make sure whatever the product we provide is fully tested and operating optimally. We have noticed that this knowledge can also be extremely useful for customers that develop their own solutions and don’t want to invest on creating their own simulation platforms or use some external solutions that will most likely not be a perfect fit. Because our customers’ wins are our wins, we are now working on providing these solutions as Testing-as-a-Service so please contact me if you have questions or interest.

joao.cardoso@danfoss.com
"


If this sounds interesting, don't hesitate to contact Joao for more information.


Have a nice day
2
Code sharing / Re: PGN 65259 SPN 588
« Last post by macbahi on May 18, 2022, 03:08:14 PM »
Hi sir Matt,

Thank you very much.

I updated my J1939 library 400 for 510.  I found all.

Thanks for your help

Yours sincerely
3
Code sharing / Re: PGN 65259 SPN 588
« Last post by Matt_Eng on May 17, 2022, 10:29:54 PM »
They are slightly newer functions, but they are available in version 5.10 of the J1939 Library.
I've attached a small screenshot of the library tab and have added red boxes to highlight the 3 functions I mentioned.

I've also added a little picture example of how the 3 blocks work together.

-Matt_Eng
4
Code sharing / Re: PGN 65259 SPN 588
« Last post by macbahi on May 17, 2022, 07:53:33 PM »
Hello sir,

Thank you very much to answer me.

but I don't know where I find Bidirectional->TransProtocol_Rx->Parsers, and it is called CI_Parser

Thanks
With regards
5
Code sharing / Re: PGN 65259 SPN 588
« Last post by Matt_Eng on May 17, 2022, 05:31:58 PM »
Hi Macbahi,

PGN 65259 is a multipacket message with variable length.

This PGN is available under Bidirectional->TransProtocol_Rx->Parsers, and it is called CI_Parser

To receive and process the message, you'll need three blocks.
1. Req_PGN_Tx: This will be used to request PGN 65259 from the remote device
2. TP_RTS_CTS_Rx: This is used to receive the multipacket messages. It needs to be configured to receive PGN 65259
3. CI_Parser: This block is connected to TP_RTS_CTS_Rx and decodes the message into a nice friendly signal.

There is a small J1939 Example in the update center that shows the CI_Parser, but it is missing the Req_Pgn_Tx function which is needed.

-Matt_Eng
6
Code sharing / PGN 65259 SPN 588
« Last post by macbahi on May 17, 2022, 02:42:31 PM »
Hi!

I want to use PGN 65259 SPN 588 in order to get engine serial number but I didn't find this function in Danfoss library.

So I must to do any alternative to get it.

I didn't understand:   stat byte = c and length =200 byte  .  Please see the file included.

Please anyone have any ideas what might be the issue?

I will appreciate your collaboration if you have a similar code to share.

Thanks in advance for your help

With best regards
7
Controllers / Re: Reading program from controller
« Last post by G30RG3 on May 17, 2022, 01:41:51 PM »
Hi,

I'm sorry, but without the source file, you won't be able to recompile and so switching an output port is not that easy.
The same goes for duplicating the controller: You need at least the compiled software, the parameter settings and passkeys to program and parameterize the controller.
I don't believe there is a way to extract the .LHX (compiled package) or back up the parameters if they're behind a passkey
8
Controllers / Reading program from controller
« Last post by michaeldostie on May 16, 2022, 06:03:32 PM »
Hi, I am new to Danfoss controllers and I have an issue with a MC-050­.

I am very familiar with OMRON and Schneider Momentum PLCs and their programming tools, but can't seem to figure out how to read or write to the Danfoss controller. One of the outputs seem to be burned out and I would like to change the mapping of the controller as I am sure they aren't all used, but I do not have the original programming as it was built by a manufacturer that does not exist anymore. Changing the unit is not a solution I want to explore either as I can't order one from them or get the original programming, and starting from scratch seems pretty ludicrous. In that case I would strip anything danfoss related and replace with what we use elsewhere.

Purchasing a license is not a problem if it is indeed what it takes, as I am guessing you can't do much with the trial version of the plus1 suite, but I want to make sure before buying anything and I am willing to learn how to use these tools. I have the usb modem and am able to connect to the controller via canbus. I see it connected.

I cannot find any relevant documentation or videos online on how to upload whatever is inside, any help would be greatly appreciated!

Have a good day


9
Controllers / Re: Controller Output diode
« Last post by FluidPowerTom on May 16, 2022, 05:40:13 PM »
Some relays can be ordered with built-in internal diodes.  I would check the relay to see if it indicates a diode on the diagram on the relay.  Otherwise you'll want to verify with the part number.  Same goes for valve coils.

However, modern microcontrollers such as PLUS1 generally do not require you to use valve coils or relays that have the diode.  That's really only needed now when you're controlling the coil with a PLC or a mechanical switch.
10
Controllers / Re: Controller Output diode
« Last post by G30RG3 on May 12, 2022, 11:55:21 AM »
As far as I read this, the "optional diode" is external.  There are internal diodes and they are always present.
Pages: [1] 2 3 ... 10