Author Topic: Can messages to a TECO vfd?  (Read 5851 times)

bgtwuk

  • Guest
Can messages to a TECO vfd?
« on: November 21, 2015, 11:34:10 PM »
Hi all.

Has anyone had experience writing can to a TECO drive to control all parameters?


Coulkd use some pointers.

Bgtwuk

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: Can messages to a TECO vfd?
« Reply #1 on: November 24, 2015, 11:28:30 AM »
Hello,

I have no experience with the TECO drive, but if it supports CANopen, it is easy to configure the Parameters on the TECO drive with a Plus+1 Controller or Display by using the right Messages and the Tx/Rx blocks in Guide.


KR,
Florian