PLUS+1 Software > Code sharing
J1939 Receiving Large Message (EC, FEE3)
nikomas:
Hi,
I have downloaded PLUS+1 GUIDE examples->J1939_Example from Update Centre 1.0.167. and implemented it in order to
receive DM01, DM02, CI and VI messages. Messages are time triggered and sent from PCAN application.
Local address is "5" (DM430 display) and source address "0".
I can receive DM01 and DM02 messages but nothing I can see on RTS_CTS_Msg bus on the checkpoints and on checkpoint after CI_Parse block.
If someone can help I will be very grateful.
Best regards,
Navigation
[0] Message Index
[*] Previous page
Go to full version