PLUS+1 Tools > PLUS+1 GUIDE
ERROR 587
(1/1)
hleppero:
I am getting this on a project after updating to 2024 version
*** ERROR 587 *** [PLUS1_IDE] INTERNAL: Unexpectedly reached else in {TXmifPresenter.GenerateOutput}
Same project was working fine in 2023 version. What is wrong?
Camox:
Hello,
I have the same errors after little modifications in a software.
Do you have a solution ?
Guide version : 2024.4.3
Tor:
Hello,
I have looked through some of the cases with this "Error 587" but have not come to any conclusion with only the information provided.
Some things to test. Please do a back up first!
1) Check if there are any non latin characters in the project path.
2) If the project is located in a synced network folder (OneDrive), please copy it it to a local folder and compile. If it's a Display project, the build folder (introduced in v2023.3.3) might be in a synced folder (GUIDE > Setup > Options > Compilation, look at the build folder path). If changing the path, copy the existing path in case you want to go back.
If this doesn't help, please contact PLUS+1 Helpdesk: https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/?plus1_product=guide
They will probably ask for the application to do some test.
Have a nice day.
Camox:
Hello Tor,
Thank you for your response.
I found a solution by creating a new project and copying the contents of the program in error.
For information, this is a project I've been working on for several weeks and the path is identical.
Have a nice day!
Camox:
I'm replying to this post following new occurrences of this error.
After a request to support, the problem has been solved by deleting characters such as accents in the Guide project path.
I hope this helps.
Have a nice day!
Navigation
[0] Message Index
Go to full version