PLUS+1 Hardware > Controllers
PVEA Error signal
(1/1)
SorenHPedersen:
Hi
I 'am new using the Sauer Danfoss controllers and have just made my first hardware setup using a MC088 and 9 PVEA valves. But for one PVEA my Error signal jumps to about 9V when I connect it to my input "C1p07_DigIn".
If I leave the input not connected the PVEA still works. It's the same if I switch PVEA's
Any idea?
Søren
Daniel:
Hi Søren,
Sorry for the late reply.
If you are still facing issues with this, I suggest you send your application (as a P1P) into helpdesk (plus+1helpdesk@danfoss.com), together with a detailed description (screenshots are also always very good), then we can have a look at it.
Best regards
Daniel
PLUS+1® HelpDesk
Navigation
[0] Message Index
Go to full version