PLUS+1 Hardware > Controllers
Pin output configuration
(1/1)
MimmoA:
Hello,
I need to use the joystick input to have an output in mA .
I scaled the Xaxispsn (-10000/+10000) with the range i need for output 200/560 mA.
Which pin do you advice me for this situaion?Is there a difference?
And how do I have to set "Outputvalue" and "pinconfig" in the pin?
Thank you so much in advanced,
Mimmo.
MimmoA:
Solved..... ;D ;D
I setted Ouputconfig with a "4" value.
Thank you
Navigation
[0] Message Index
Go to full version