PLUS+1 Hardware > Controllers
Reading the RPM from an engine alternator W signal
(1/1)
240glt:
Hi.
I need to get the engine RPM from an diesel engine, with pure mechanical injection (no engine ECU). There is an alternator with W signal. I have looked at the signal with an oscilloscope, and it looks like the attached photos: -30V to +34V, 167Hz at idle, and 400Hz at 2000rpm. That voltage levels is not quite perfect for the MC024-010 controller that I intended to use.
Have anyone of you made something similar? Do I need to have diodes to limit the voltage levels, or is it enough with just the resistor? I guess that there is diodes in the controller input, maybe that is enough if I use a high resistance (like 100k) to limit the current?
Thanks!
240glt:
I forgot to attach the schematic of what I hope that I don't need:
Neil:
Hi.
I have read the W pin as a Straight Freq and Per into controllers without any issues.
regards Neil.
Jakob:
Hello
The diesel engines I usually work with are using a 24V alternator, and I have also just connected the W signal direct to the MC input.
It has worked without any problems.
What battery voltage is your system running at?
regards Jakob
240glt:
Thanks, that will make it easier! I was just a little bit worried, as the specification says "Allowed voltage at pin 0-36VDC". And I have negative 30VDC half of the period.
Yes, it's a 24V system.
Thanks!
Regards
Kent
Navigation
[0] Message Index
Go to full version