Author Topic: Mc038 Power pins  (Read 4564 times)

bgtwuk

  • Guest
Mc038 Power pins
« on: September 17, 2013, 06:57:47 PM »
Gents

On the MC 038, are the power pins 36, 37, 38, connected internally together?

Are they connected to pin 2?

Can I monitor them individually for voltage available? Will I need to connect my source for each also to a input to monitor?
Thanking you in advance.

Bgtwuk

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Mc038 Power pins
« Reply #1 on: September 18, 2013, 03:57:49 AM »
They are independant.
They are not connected to pin 2.
Each one is assigned to output pins as per the Datasheet.
Each input voltage can be monitored individually.

bgtwuk

  • Guest
Re: Mc038 Power pins
« Reply #2 on: September 18, 2013, 03:27:56 PM »


I believed that to be true, based on the datasheet.

When I connected the module to my power supply, using only pin 1 and pin 38, the module powered up.

Of course this is upsetting when the plan was to isolate the power pins so the trace from pin 2 does not burn off.