Recent Posts

Pages: 1 ... 6 7 [8] 9 10
71
PLUS+1 GUIDE / Re: Missing fonts error when trying to compile with 2024.1
« Last post by williamk on March 06, 2024, 06:08:52 PM »
This appears to be fixed in 2024.1.4
72
Controllers / Re: Parameters not visible
« Last post by SVK on March 06, 2024, 01:42:51 PM »

I found what was wrong.
The OS was different, all parameters became visible when I updated the OS.

Thx for the help though.
73
Controllers / Re: Parameters not visible
« Last post by Tor on March 06, 2024, 08:25:09 AM »
Hello SVK,

If you open the service application in an earlier version of Service Tool does it work?
In that case I would recommend you to create a case for PLUS+1 Helpdesk:  https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-support

If there have been a name change for some reason, you need to open the service screens and change the signals to the correct ones. I have marked in the attached image where to look when using a regular parameter component in Service Tool.
If you don't have permission/access to do this, I would recommend you to contact the developer of the service screens or the machine manufacturer.

Have a nice day,
74
Controllers / Parameters not visible
« Last post by SVK on March 05, 2024, 01:45:35 PM »
Hi all,

I have a project file that dates from 2016. When I open it in the latest Plus+1 service tool some parameters are not shown because they don't exist or have another name.
How can I fix this issue?

The parameters I haven't found yet are:
EE_DOutSpd_rpm1
EE_DOutTorque_Nm3
EE_MagCurrBoost_pct2
EE_SnsrSupplyVltg
EE_SpeedCalcMode
EE_SpeedFOF_ms
EE_VCellRst_mV
SpdInvSgn
Val1 To Val10
75
Displays / Re: Lifetime NVmem Erase/Write for DM430E
« Last post by Tor on March 05, 2024, 01:41:32 PM »
Hello,

Sorry about the late response.

I was approached by a developer who saw this topic and he wanted me to write a clarification to avoid confusion.
When it comes to the DM430 and the EEPROM we guarantee 4 million write cycles.


Have a nice day.
76
Displays / Applog size and memory usage
« Last post by Lukey on February 29, 2024, 06:35:03 AM »
Hello, i am using a DM1200T.

Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?

Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.

The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.
77
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Egholm-Jonas on February 28, 2024, 01:32:21 PM »
With some help from Tor, I can move on again!! :)

The invalid character '0xBB" error was caused by the checkmark in "Regions Settings" on my pc. (See attached picture)

Why this was selected I have no idea! But this did it for me! :)
78
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by acmall on February 26, 2024, 12:03:55 PM »
I just did a test on two projects, one using a DP720 and the other MC088-015. Both complied without issues and appear to be producing working programs on a bench test.

It would be good to find out what is causing this issue for some uses. For reference the HWD files for the programs I tested are: -
MC088-015 = V200
DP720 = tested with booth V260 & V270.

79
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Egholm-Jonas on February 26, 2024, 11:38:22 AM »
Hi Camox,

Nothing out of the ordinary!
Except updating to the new Guide 2024.1.3

Yes, I have a 1 month old backup! :'(

If I create a new Application, I does the exact same!
80
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Camox on February 26, 2024, 11:09:17 AM »
Hi, there,
What changes did you make after the previous compilation?
Do you have a backup with the 2023 version of the Guide?

Have a nice day!
Pages: 1 ... 6 7 [8] 9 10