PLUS+1 Hardware > Displays
DM430E flashing issue
(1/1)
george:
Hello,
With the Plus+1 trial license I could flash and reflash a test application into the DM430E-0-0-0-0 display.
When the trial license expired, I switched to an express license and since then I am facing issues in reflashing the display.
I am not sure I am missing any additional project settings in my project configuration.
Could you please help?
The display is connected through the host PC using PCAN hardware with RP1210C driver.
Refer "Screenshot_1.png" for the gateway configuration.
Refer "Screenshot_2.png" for the system scan that recognised the display device.
Refer "Screenshot_3.png" for download file to ecu.
Thank you very much in advance.
george:
Any thoughts?
This is a stopping issue and I am unable to get it resolved.
Is there any technical team I can talk to or an email where I can email the issue further?
Thanks.
sverreo:
You can reach out to the helpdesk if you have any issues:
https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/
Make sure you only have 1 display connected with the same Node ID. If you have more than 1 unit with the same Node ID connected you can get this error.
Also make sure you have the CAN terminated properly with 120ohm in both ends of the bus.
george:
Thank you sverreo for your suggestion. It helped to re-flash the display.
I didn't realise I need to add a third node on the system in order to complete the flash sequence as per Screenshot_4.png.
I added a second PEAK hardware with a different device ID and it allowed me to complete the flashing.
I will write a detailed instruction later for the benefit of others.
Navigation
[0] Message Index
Go to full version