Author Topic: EMD Speed Sensor  (Read 16061 times)

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 117
  • Karma: +6/-1
Re: EMD Speed Sensor
« Reply #15 on: May 01, 2020, 04:50:02 AM »
It depends on the control precision you want to achieve. In your example, you told us about a 200 RPM target and the RPM seen by the sensor were in the 199.0 to 203.6 range. This is an error of -0.5% / +1.8%, which is not too bad in my opinion.

Sam