PLUS+1 Tools > PLUS+1 GUIDE
Pulse which holds sinal for duration even if input signal goes T/F.
(1/1)
ET:
The help docs state that the Pulse component will output false if the input goes T/F during the hold time.
Is there another component which will continue to output true for the entire hold time, even if the input goes T/F during the hold time?
If not, is there an easy way to wire this function up using other components?
A.Peterson:
Use a positive transition into a delay off and you can set the length of pulse to whatever you want regardlees of the input state.
ET:
Ah, that sounds like it will work nicely.
Thanks!
Navigation
[0] Message Index
Go to full version