Author Topic: HMR MAX COUNT ROTARY ENCODER  (Read 3657 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
HMR MAX COUNT ROTARY ENCODER
« on: March 25, 2020, 09:12:27 PM »
Hey Guys,

does anyone knows where to get the HMR service tool file to set the maximum count of the rotary encoder?

as per datasheet there is one, I just cannot figure out where to get it from.

Thanks for the advise


Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: HMR MAX COUNT ROTARY ENCODER
« Reply #1 on: March 26, 2020, 11:56:38 AM »

Hi,

Check under the hardware tab under HMx. Find the Misc Files folder.



Right click on the file and select Copy To Clipboard.
Then open PLUS+1 Service Tool and create a new service application. Right click on the parameters page and then choose Import from clipboard.


Best regards,
Tor
PLUS+1® SW PAE Team

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: HMR MAX COUNT ROTARY ENCODER
« Reply #2 on: March 26, 2020, 01:18:27 PM »
Hi,

I hope the Image work now....
Best regards,
Tor
PLUS+1® SW PAE Team

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: HMR MAX COUNT ROTARY ENCODER
« Reply #3 on: March 26, 2020, 03:13:08 PM »
alright!!

that works, I tried it before just by double click but it did not work becuase it was not the correct procedure

Thanks