Daniel,
Just one more question,
if I have my check points at the display and I am connected to the CAN and the DP610 using the USB/RS232 cable going from the back of the display to the laptop, does those checks points only are access/transmitted over the USB connection for logging with the service tool?
in other words, under the same set up, if I got check points at the controller they will be requested and transmitted on the CAN bus and then on the USB right?
but for the DP610 what does really happen when trying to request/transmit the checkpoint info to the service tool log?
Iam asking this because after all if everything has to go to on the CAN BUS, it will impact my bus load
I appreciate the feedback
Regards