Author Topic: Basic FB Library with Pro Trial not showing up  (Read 7698 times)

Offline Jerry B

  • PLUS+1 User
  • **
  • Posts: 9
  • Karma: +0/-0
Basic FB Library with Pro Trial not showing up
« on: August 17, 2018, 08:33:03 PM »
I am missing the Basic FB library that is supposed to come with the Pro license. I was able to download a bunch of the other libraries, but would like to use the CAN blocks from the Basic Function Library. Is there somewhere to download the Basic Library, I did not see it on the PLUS+1 Libraries page with all the other downloadable libraries.

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Re: Basic FB Library with Pro Trial not showing up
« Reply #1 on: August 20, 2018, 08:55:57 AM »
I don't think the Basic Function Block library exists anymore. The functions were split out into the Controls, Inputs, Outputs, & Filters Libraries.

Alastair

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Basic FB Library with Pro Trial not showing up
« Reply #2 on: August 21, 2018, 09:22:06 AM »
Hi guys!

Alastair is correct in what he is saying Jerry; the basic function library doesn't exist as a whole anymore but is devided into Controls, Inputs, Outputs, & Filters Libraries. All found under one tab here on our website;

https://www.danfoss.com/en/products/software/dps/plus1-software/plus1-libraries/#tab-overview

The CAN blocks on the other way are not included in any of these libraries anymore but moved into the components tab found under Connection->CAN and there you have one for Transmit CAN and three different ones for Receive CAN (with Filter/with ID Mask/Basic).

I hope this helps!

Best regards
Nilla
PLUS+1 Helpdesk team