Recent Posts

Pages: 1 2 [3] 4 5 ... 10
21
Displays / HELP - I accidentally closed my project manager tab..
« Last post by BBarry on September 08, 2022, 09:18:35 PM »
HELP - This seems dumb but I accidentally closed my project manager tab.. and now I cant get it back. The manual says that "In the View menu, click Default Layout to display the Project Manager and Inspector tabs" but there is not such option in view.

For that matter I unsnapped another tab and it wont re-integrate when I put it on the edge of my screen.

This is killing me I am trying to wrap up this program and I cant copy and delete the screens I need to.

Please Help!
 :o
22
Displays / Re: Real Time Clock For DM430
« Last post by BBarry on September 08, 2022, 09:13:45 PM »
Thanks That helped a lot!!!
23
Displays / Re: Download time in DM1000
« Last post by Camox on September 07, 2022, 08:05:11 AM »
Hello Thor,
Thank a lot four your response.

I’ll get that cable fast.

Have a nice day
24
Displays / Re: Download time in DM1000
« Last post by Tor on September 07, 2022, 07:29:18 AM »
Hello Camox,

Yes the download time for the DM1x00 displays are a bit longer than the rest of units. Especially when you are replacing the HWD file and OS.
I recommend to use USB when working with the DM1x00 displays. You will save a lot of time. When it take almost an hour downloading a new OS with CG150, it will only take a minute with the USB.

If you want to order you can find the part number in the image below (11231512). You can also find it in the Data Sheet.


Have a nice day.
25
PLUS+1 GUIDE / Re: Installing V260 Display hardware files in Guide 2022.2.5
« Last post by Fredrick on September 06, 2022, 08:09:16 PM »
Works for me to to.
When I deleted the BookCase.xml file I successfully could update the HWD file for DM430E display.
26
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on September 06, 2022, 08:07:31 PM »
Thank you for the information. :)
27
Displays / Download time in DM1000
« Last post by Camox on September 06, 2022, 04:44:15 PM »
Hello,
I work actually on software for DM1000 dysplay.
The download time for add a software in the dysplay in long. During the download the load speed on the dyspaly is 10kb/s.

We can change the load speed ?

Thank in in advance.

Good day
28
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Tor on September 06, 2022, 03:42:32 PM »
Hello,

This issue is reported (P100006351) and will be fixed in the next release.
I recommend to use the 2022.1 until this is fixed.

Sorry about the inconvenience.
29
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on September 06, 2022, 10:57:07 AM »
Anyone else having problems with this?
Also, sometimes the P1D file does´t get saved so next time you open the P1D file the changes are lost and you now have an older P1D file without the changes you just did. :(
30
Displays / PIB - DM1x00 HWD file update
« Last post by Tor on September 02, 2022, 10:07:18 AM »
Hello,

If you have not seen the latest PIB (Product Information Bulletin) about the DM1x00 I would like to share it here.

In short:
An issue was found that can cause the device to lock and become unrecoverable. The advice is to recompile to .HWD v308 or greater for any devices with a manufacturing date of August 11 or after.
The HWDs are located in the PLUS+1 Update Center. The version stated in the Update Center is 3.8.0 for some reason, but it's v308 when installed in GUIDE.

More information in the attached image/PDF file.


Thank you.
Pages: 1 2 [3] 4 5 ... 10